AnsweredAssumed Answered

Multiple JTAG Targets?

Question asked by nate.domin on May 21, 2014
Latest reply on May 21, 2014 by PatrickN

I'm confused by the JTAG output scans of an EVAL-ADUC7023QSPZ1 board. -- According to the schematic, the U5 (FT2232HL) is disconnected from the JTAG lines.  But when inspecting the JLink.exe output I see 2 JTAG devices:

 

PS C:\Program Files (x86)\SEGGER\JLinkARM_V484e> .\JLink.exe -Device ADUC7023

SEGGER J-Link Commander V4.84e ('?' for help)

Compiled Apr 28 2014 20:50:11

Info: Device "ADUC7023" selected (62 KB flash, 8 KB RAM).

DLL version V4.84e, compiled Apr 28 2014 20:50:02

Firmware: J-Link ARM V8 compiled Nov 25 2013 19:20:08

Hardware: V8.00

S/N: XXXXXXX

OEM: MIDAS

Feature(s): RDI, GDB

VTarget = 3.287V

Info: ADI system TAP: Connecting to device with system TAP.

Info: TotalIRLen = 5, IRPrint = 0x11

Info: Analog devices system TAP: Enabling CPU core.

Info: TotalIRLen = 9, IRPrint = 0x0011

Found 2 JTAG devices, Total IRLen = 9:

#0 Id: 0x4F1F0F0F, IRLen: 04, IRPrint: 0x1, ARM7TDMI-S Core

#1 Id: 0x028011CB, IRLen: 05, IRPrint: 0x1, System level TAP

Found ARM with core Id 0x4F1F0F0F (ARM7)

RTCK reaction time is approx. 504ns

Using adaptive clocking instead of fixed JTAG speed.

 

What is the second JTAG device?   A preliminary inspection of R35, R36, R37, R38 shows that they are not populated (by design).

Outcomes