AnsweredAssumed Answered

Rules for multiple SPI write cycles in succession

Question asked by jgmick on May 20, 2014
Latest reply on May 20, 2014 by NevadaMark

What are the timing limits to send multiple configuration commands to the ADIS16364?  Can I send some arbitrary number of SPI command cycles within the same frame of 1 cycle of SS* HIGH to LOW to HIGH or does each transmission require an independent SS* cycle?  If multiple cycles are allowed I would assume a reasonable time of 1 uSec minimum between the last clock rising edge of SCLK of a SPI cycle and the first clock falling edge of SCLK of the next SPI cycle.  Is this a valid assumption or is a longer wait necessary?

Outcomes