AnsweredAssumed Answered

ADV7623-P and Bypass_Audio_Passthru

Question asked by caw97 on May 20, 2014
Latest reply on Jun 2, 2014 by mattp

Hello,

 

We're using the ADV7623-P (non-HDCP variant) in a design and we are trying to "inject" audio into the HDMI_Tx stream.  However, the audio seems to always be in passthru mode, regardless of what value we write to Rx_HDMI_MAP register 0x3C (BYPASS_AUDIO_PASSTHRU).  ie We can write 0x12 or 0x02 to Rx_HDMI_MAP 0x3C and in either case the audio gets passed through.

 

Is there another register or setting that overrides the BYPASS_AUDIO_PASSTHRU bit?

 

We are trying to inject 24-bit 48kHz 2-channel I2S (left-justified) audio via AP1_In (pin 76), using AP5_In (pin 70) as the LRCK, SCLK_In (pin 69) as the bit-clock and MCLK_In (pin 68) as the master clock.  Master clock = 12.288MHz.  Everything looks good at the corresponding pins, but the Tx audio is always the same as the Rx audio and not what we're injecting.

 

Any help is much appreciated.  Thanks!

Outcomes