AnsweredAssumed Answered

ADV7610_reference_oscillator_pin

Question asked by AdrianB on May 20, 2014
Latest reply on May 28, 2014 by edo

Hello,

I am developing  a video processing board using ADV7282M decoder and ADV7610 HDMI receiver. Due to the fact that both use the 28.63636 MHz clock, I intend to use a single 1.8 V reference oscillator. My problem is the following:

In the ADV7282M datasheet (page 10). the input for the reference oscillator is XTALN, while in the ADV7610 datasheet (page 9) is indicated XTALP. It's a mistake in the datasheet or the two mentioned circuits have different hardware structure...?

 

Thank you !

 

AdrianB

Outcomes