AnsweredAssumed Answered

ADF7021 Daughter board ADF7021DBZ5

Question asked by RoggerOA on May 19, 2014

Hi,

 

I have this daughter board (ADF7021DBZ5) which i will stream to 144 MHz, then my question is, which components I need on this board to transmit at the desired frequency?, Since this board does not come with the necessary components to transmit.

 

 

In the application note AN-859 there are a components of the band 140-150 MHz, but on page 10 is the use of an XTAL of 11.0592 MHZ and ADF7021DBZ5 board comes already connected to 19.680 MHz XTAL.

 

So my question is: which components they need connect on this card to transmit a 144 MHz to 19,680 MHz XTAL?

Outcomes