AnsweredAssumed Answered

custom waveform not loading

Question asked by mgm on May 15, 2014
Latest reply on May 27, 2014 by larsc

I have a custom waveform with 76802 samples (10 ms duration at 7.68 MHz sampling rate for a 5 MHz spectrum). I am trying to load this waveform for the Tx in an AD9364/ZC702 demo and it is not loading.

I reduced the number of samples in the file from 76802 to 46082 and the waveform seems to be loading.

 

Please help me with the following questions:

- What is the reason for which the waveform with 76802 samples is not loading? What do I need to do to make it load?

- What is the maximum number of samples supported on the ZC702 platform for custom waveforms for Tx?

 

-- Mihai

Outcomes