AnsweredAssumed Answered

ADP5065 battery current

Question asked by David.A on May 14, 2014
Latest reply on Aug 15, 2014 by GYang

Using the ADP5065, what is the current consumption from the battery when Vin=0 (isolation FET conducting)?  I see a spec for "Battery, Standby" in the current consumption section of the datasheet, but I could not find any definition of "Standby".  Put another way, if the USB is not connected, the battery is at 3.6V, and the system is using 10uA, what is the load on the battery?  Thanks.


Outcomes