AnsweredAssumed Answered

discontinuous custom waveform

Question asked by mgm on May 13, 2014
Latest reply on Jun 4, 2014 by larsc

I loaded a custom waveform into the AD9364/ZC702. The waveform in the file is a continuous signal of 10 ms duration, but when I measure what the transceiver generates it appears with time-slots of approximately 2 ms.

The original signal is an LTE FDD 5 MHz, so I also used the LTE5_MHz filter that came with the demo board.

Please help me understand whay the signal is not continuous.

I attach two images with the signal in the file (continuous) and the signal measured at the output of AD9364 (not continuous).

 

Thank you,

Mihai

Outcomes