AnsweredAssumed Answered

ADSP-BF609 DEBUG  error --Failed to connect to Processor

Question asked by zhoudezhi on May 12, 2014
Latest reply on May 12, 2014 by DavidS

Hi!

I'm recently experiencing problems with ADSP-BF609 when I try to Program ADSP-BF609 via ICE-100B emulator,the BF609's version is v0.1

and CCES's version is 1.0.3

 

I Get this message :

 

[TpsdkServer] Failed to connect to processor.

 

Error: 0x8004804a

Error Description: Detected number of device does not match settings

 

I have Read the Emulator and Evaluation Hardware Troubleshooting Guide for

CCES Users,and there is no information about this error code.

I try to disconnec the emulator to my target board  and The message changed,as Below:

[TpsdkServer] Failed to connect to processor.

Error: 0x80048049

Error Description: Failed detecting number of device connected

 

I have done the ICE test and the ICE test result As Below:

Open emulator interface:Successe

Resetting ICEPAC module :Successe

Testing ICEPAC memory:Successe

Determing scan path :error

 

Any one has seen this problem before?

What should i do to solve this problem?

 

Best Regards

Beck Chow

 

 



 

Outcomes