AnsweredAssumed Answered

USB problem on BF609 ezkit

Question asked by hichem on May 9, 2014
Latest reply on Sep 12, 2014 by hichem

Hi,

 

I'm using the blackfin buildroot 2013 R1 RC2 version.

When I have activated the USB driver following the steps figuring in the link below:

http://blackfin.uclinux.org/doku.php?id=linux-kernel:drivers:musb&s[]=blackfin&s[]=usb&s[]=driver

 

I have received the error below when the board boots (see the attached file):

"musb-hdrc musb-hdrc.0.auto: musb_init_controller failed with status -517"

 

Please which are the kernel config to set to be able to detect an usb mass storage?

NB: I'm using an USB adapter which support the OTG.

 

Thanks in advance.

Attachments

Outcomes