AnsweredAssumed Answered

FMCOMMS2 and Vivado 2013.4 HDL Reference Design

Question asked by Quamstar on May 8, 2014
Latest reply on Aug 20, 2014 by rejeesh

Hey Guys,

 

regarding to this http://ez.analog.com/thread/39693 Discussion, i would like to push this Topic. I tried to build the Librarys for the AD9361 and the Project fmcomms2 from https://github.com/analogdevicesinc/hdl into Vivado 2013.4, as well as 2014.1 but in any cases i become the following error by building the project. By the way i tried the instruction onhttp://wiki.analog.com/resources/fpga/docs/hdl/vivado

 

...

### set axi_iic_main [create_bd_cell -type ip -vlnv xilinx.com:ip:axi_iic:2.0 axi_iic_main]

### set_property -dict [list CONFIG.USE_BOARD_FLOW {true} CONFIG.IIC_BOARD_INTERFACE {IIC_MAIN}] $axi_iic_main

 

 

ERROR: [BD 5-216] VLNV <analog.com:user:util_i2c_mixer:1.0> is not supported for this version of the tools

ERROR: [Common 17-39] 'create_bd_cell' failed due to earlier errors.

 

    while executing

"create_bd_cell -type ip -vlnv analog.com:user:util_i2c_mixer:1.0 sys_i2c_mixer"

    invoked from within

"set sys_i2c_mixer [create_bd_cell -type ip -vlnv analog.com:user:util_i2c_mixer:1.0 sys_i2c_mixer]"

    (file "../../../projects/common/zed/zed_system_bd.tcl" line 64)

 

    while executing

"source $ad_hdl_dir/projects/common/zed/zed_system_bd.tcl"

    (file "system_bd.tcl" line 2)

 

    while executing

"source system_bd.tcl"

    (procedure "adi_project_create" line 88)

    invoked from within

"adi_project_create fmcomms2_zed"

    (file "./system_project.tcl" line 7)

 

Does anybody had already problems like this and can provide a solution?

 

Thanks and regards

Jan

Outcomes