AnsweredAssumed Answered

ADE7953 UART problem

Question asked by semansky@zapsi.eu on May 6, 2014
Latest reply on Feb 19, 2018 by knesargi@dovercorp.com

Hello, did any use UART interface on ADE 7953?

When I select SPI comunication every thing is OK, but on same board when I select UART comunication, I don't get aby answer from ADE7953.

 

For UART select I put pin 28 ( CS ) to 3V3 and  pin25 (SCK) to GND. And then I try read any register, for example CONFIG reg at adress

0x102.

I send to UART (at speed 4800 baud)  this: 0x35 0x01 0x02 and after t2 (6ms) I should get answer from ADE7953. But I don't get anytihmg.

At pin26 (TX pin of ADE) is still HIGH and no activity.

 

Have anybody succesfull comunication with this UART?

Outcomes