AnsweredAssumed Answered

ADuC7061 VIC Example for uVision 4?

Question asked by K.T.Eng on May 5, 2014
Latest reply on Jun 1, 2014 by K.T.Eng

I am trying to implement VIC for a project and i am a little bit stack.

What ever I do the interrupts handlers are not called, the program interrupts are always going to the void IRQ_Handler(void) __irq function.

My project compiles but it seems to me that there is a conflict between irq_arm.c interrupt and the vic.c interrupt.

 

Can you please provide me with a simple project using VIC in C that compiles in uVision 4 and using different interrupt handlers for ADC or UART for example?

 

I would appreciate the example as i cannot find one in the net that is actually working in the uVision 4.

Outcomes