AnsweredAssumed Answered

ADV7611 configuration for 1080p 4:2:2 8bit

Question asked by zhutousame on May 5, 2014
Latest reply on May 7, 2014 by zhutousame

Hi,

We are using ADV7611 in our project. We have HDMI interface on our board.We want to capture 1080P60 video with 422 and 8bit .

here  is my REG script.

 

0x98   0x01   0x06 

0x98   0x02   0xf2  //

0x98   0x03   0x00  // 8bit sdr 656 mode

0x98   0x05   0x28  // AV Codes Off

0x98   0x06   0xa6 

0x98   0x0b   0x44 

0x98   0x0c   0x42 

0x98   0x15   0x80 

0x98   0x19   0x8a 

0x98   0x14   0x7f 

0x98   0x33   0x40 

   

0x44   0xba    0x01    

   

0x64   0x40    0x81     

   

0x68   0x9b    0x03  // ADI recommended setting

0x68   0xc1    0x01    

0x68   0xc2    0x01    

0x68   0xc3    0x01    

0x68   0xc4    0x01    

0x68   0xc5    0x01    

0x68   0xc6    0x01    

0x68   0xc7    0x01    

0x68   0xc8    0x01    

0x68   0xc9    0x01    

0x68   0xca    0x01    

0x68   0xcb    0x01    

0x68   0x00    0x00    

0x68   0x83    0xfe    

0x68   0x6f    0x08   

0x68   0x85    0x1f    

0x68   0x87    0x70    

0x68   0x8d    0x04    

0x68   0x8e    0x1e    

0x68   0x1a    0x8a    

0x68   0x57    0xda    

0x68   0x58    0x01    

0x68   0x75    0x10    

     

//////////////////////////////////////////////

but the yuv displays like this:

hdmi_input.jpg

The source is like this

src.jpg

 

I am wondering there is something wrong with my configuration.

Regards,

Ben

Outcomes