AnsweredAssumed Answered

About Input voltage range

Question asked by Tarzan on May 1, 2014
Latest reply on May 9, 2014 by Tarzan

Hi there,

I have a quesion about AD8691.

http://www.analog.com/static/imported-files/data_sheets/AD8691_8692_8694.pdf


Looking at the input voltage range of the datasheet, it says +3.9V(Max) at Vs=5V.

And also this is  specifired at T A  = 25°C.

I need information on input voltage range when Ta is  between -10℃ and +50℃.

Do you have the data on that?

Over the temparete, how much do you think input max range would change?

 

Thanks in advance.

 

Best regards,

Tarzan

Outcomes