AnsweredAssumed Answered

ADP1046 capability

Question asked by Mack on Apr 29, 2014
Latest reply on Apr 30, 2014 by xudong

Hello,

 

I consider designing two DC-DC power systems.

One is 2kW power.

     input: 250V~450V

     ouput: 10V ~ 16V, 150A

 

The second is 10kW.

     input: 350V ~ 450V

     output: 350V ~ 450V, 28A ~ 22A

 

Is both possible to design with ADP1046?

 

Best Regards,

Mack

Outcomes