AnsweredAssumed Answered

ADV7842 connected to ADV8003, Test4, Test5, Test8

Question asked by danngai on Apr 29, 2014
Latest reply on Apr 30, 2014 by DaveD

Hello,

 

Planning on designing with ADV7842 connected to an ADV8003.   In creating the schematic for this, I have referenced the Datasheet; the ADV7842 Eval Schematic; and ADV8003 Eval Schematic and they are all showing something different for hooking up Test4, Test5, Test8.  I've listed the conflicts and referenced the pdfs that I used.   Which one is the correct?   Thank you!

 

Dan

 

ADV7842  Data Sheet  http://www.analog.com/static/imported-files/data_sheets/ADV7842.pdf

  • TEST4:   P. 18  "Connect this pin to GROUND"
  • TEST5:   P. 18  "Connect this pin to GROUND"
  • TEST8:   P. 14   "Tie this pin TO GROUND VIA 4.7K RESISTOR"

  

ADV7842 Eval Schematic SHEET 7.  http://ez.analog.com/servlet/JiveServlet/download/1681-13-4521/EVAL-ADV7842-7511_Rev1p0.pdf

  • TEST4:   FLOATING
  • TEST5:   FLOATING
  • TEST8:   NOT SHOWN

 

ADV8003 Schematic SHEET 16.   http://ez.analog.com/servlet/JiveServlet/download/4497-2-18569/EVAL-ADV8003-SMZ-P_schems_20130809.pdf

  • TEST4:   GROUND
  • TEST5:   FLOATING
  • TEST8:   CONNECTED to 3.3V VIA 4.7KOHM RESISTOR.

Outcomes