AnsweredAssumed Answered

Running multiple applications on BF537

Question asked by AsifHabib on Aug 9, 2010
Latest reply on Jan 17, 2017 by MattZ

Hi,

 

I want to download multiple BF537 VDK applications to the on-board flash of my custom board, and then run the applications simultaneously on the BF537 processor. Although some description is given regarding this in VDSP loader manual but it is not clear to me. If someone could explain following to me?

 

1) How to program BF537/flash with multiple .ldr files which I want to run on the DSP?

2) Which application will boot first? Can all of them run simultaneously and perform their independent tasks?

3) Both will be able to access same PORT e.g. both can access the UART sequentially if applications run simultaneously?

 

 

Best Regards,

Asif Habib

Outcomes