AnsweredAssumed Answered

ADuC7061 Source code for CN0196

Question asked by rpmarchand Employee on Apr 27, 2014
Latest reply on Jun 18, 2014 by MMA

Hello!

 

I have the evaluation boards for the circuit from the lab #196 (http://www.analog.com/en/circuits-from-the-lab/CN0196/vc.html) and i was hoping to make some modifications to the source code placed in the ADuC7061 to be able to customize it for my application.  I have all of the boards as mentioned in the circuit note as well as the software installed.  I looked through the directories and i can only find a hex image of the firmware running on the ADuC7061.  

 

Is it possible to be able to provide either an IAR workspace or the appropriate source files?  I understand that it likely isn't that complicated to re-create the source code but it would be convenient to re-use the code you already have if at all possible.

 

Thanks!

Outcomes