AnsweredAssumed Answered

ADV7611, 720p In and 8bit TTL Out

Question asked by JerryS on Apr 24, 2014
Latest reply on Apr 29, 2014 by GuenterL

Hello, Sir

 

I have a customer request for ADV7611 8bit TTL output during 720p video input.

I have tried a script as below, and it is ok for 480P/480i input and 8bit TTL out.

Same script, I change input video resolution to 720P, but the output pixel clock of ADV7611 is not 148.5MHz.

Is anything I miss?

Thank you very much.

 

0x98, 0xF4, 0x80,

0x98, 0xF5, 0x7C,

0x98, 0xF8, 0x4C,

0x98, 0xF9, 0x64,

0x98, 0xFA, 0x6C,

0x98, 0xFB, 0x68,

0x98, 0xFD, 0x44,

0x98, 0x00, 0x02,

0x98, 0x01, 0x06,

0x98, 0x02, 0xF5,

0x98, 0x03, 0x00,

0x98, 0x05, 0x2C,

0x98, 0x06, 0xA6,

0x98, 0x0B, 0x44,

0x98, 0x0C, 0x42,

0x98, 0x15, 0x80,

0x98, 0x19, 0xC3,

0x98, 0x33, 0x40,

0x44, 0xBA, 0x01,

0x68, 0x9B, 0x03,

0x68, 0x00, 0x00,

0x68, 0x83, 0xFE,

0x68, 0x6F, 0x0C,

0x68, 0x85, 0x1F,

0x68, 0x87, 0x70,

0x68, 0x8D, 0x04,

0x68, 0x8E, 0x1E,

0x68, 0x1A, 0x8A,

0x68, 0x57, 0xDA,

0x68, 0x58, 0x01,

0x68, 0x75, 0x10,

0x68, 0x90, 0x04,

0x68, 0x91, 0x1E,

0x68, 0x9D, 0x02,

Outcomes