AnsweredAssumed Answered

AD-FMCOMMS1:  ML605 software hangs

Question asked by uwinprep on Apr 18, 2014
Latest reply on Apr 23, 2014 by AdrianC
Branched from an earlier discussion

Hi

 

I have a problem while running no-OS software on ML605 board connected with Fmcomms1-EBz radio card. When I run the software it hangs on at the last line "Testing the ADC communication..." as shown below. I tried a lot but couldn't succeed. I would appreciate your help. The complete output is as shown below

 

Running XCOMM Test Program

  Initializing XCOMM I2C...

XCOMM Init I2C OK!

 

Getting XCOMM Revision...

Board Version: Analog Devices, FMC Comms 1, D501462, AD-FMCOMMS1-EBZ, BOM Rev.1

 

Initializing XCOMM Components...

XCOMM Init OK!

 

Initializing the Rx path...

XCOMM Rx Init OK!

 

Initializing the Tx path...

XCOMM Tx Init OK!

 

ADC sampling rate [Hz]: 98304000

 

DAC sampling rate [Hz]: 491520000

 

DAC available interpolation frequencies [Hz]: 491520000 983040000

 

DAC available center shift frequencies [Hz]: 0

 

Testing the ADC communication...

Outcomes