AnsweredAssumed Answered

UG-065 datalogging

Question asked by dridgway on Apr 22, 2014
Latest reply on May 12, 2014 by neilzhao

Hello, I just received the UG-065 datalogger and have been able to collect data from it. I reprogrammed it with the 16G, 800Hz full resolution hex file and noticed that after one minute of data collection, the text file was over 2MB of data and after the one minute mark, the data became corrupted. Any idea what may be causing this? Also, is there another version that uses the SPI bus? I would like to be able to sample up to the 3200Hz limit. I have attached the file for viewing.

 

Thank you for your time,

David

Outcomes