AnsweredAssumed Answered

FMCOMMS1-EBZ

Question asked by uwinprep on Apr 22, 2014
Latest reply on Apr 23, 2014 by AdrianC

Hi,

 

I work with FMCOMMS1-EBZ card with ML605 xilinx board. I tried to run a reference design no-OS driver on this card. But the reference design doesn't work properly. I am using Xilinx-ISE Design Suite 14.4.The following is the output (Below), actually it stops at the line "Testing the ADC communication... ". I tried to trace it out and find that it is stuck up in the test.c file in the do statement as

do

          {

                    delay_ms(1);

            }

 

 

 

 

Running XCOMM Test Program

 

 

Initializing XCOMM I2C...

XCOMM Init I2C OK!

 

 

Getting XCOMM Revision...

Board Version: Analog Devices, FMC Comms 1, D501462, AD-FMCOMMS1-EBZ, BOM Rev.1

 

 

Initializing XCOMM Components...

XCOMM Init OK!

 

 

Initializing the Rx path...

XCOMM Rx Init OK!

 

 

Initializing the Tx path...

XCOMM Tx Init OK!

 

 

ADC sampling rate [Hz]: 245760000

 

 

DAC sampling rate [Hz]: 245760000

 

 

DAC available interpolation frequencies [Hz]: 245760000 491520000 983040000

 

 

DAC available center shift frequencies [Hz]: 0

 

 

Testing the ADC communication...

Outcomes