AnsweredAssumed Answered

Is it impossible to set Fs=192kHz for EVAL-ADAU1452MINIZ?

Question asked by kegasa2014 on Apr 21, 2014
Latest reply on Jan 1, 2016 by DaveThib

In EVAL-ADAU1452MINIZ User Guide UG-636, I found the line below.

" The AD1938 is configured to run at a sample rate of 44.1 kHz

or 48 kHz. It is not possible to change this setting. Even though

the ADAU1452 is very flexible and can run at any sample rate

up to 192 kHz, the analog audio inputs and outputs on the

EVAL-ADAU1452MINIZ may be distorted or silent if a sample

rate other than 44.1 kHz or 48 kHz is used for the ADAU1452

serial ports."

 

Is it impossible to set Fs to 192kHz when using EVAL-ADAU1452MINIZ with SigmaStudio 10.3.10 ?


Is there any easy way to wrok around this limitation?

 

I want to use EVAL-ADAU1452MINIZ to analyze 40kHz signal.

 

http://www.analog.com/static/imported-files/user_guides/EVAL-ADAU1452MINIZ_User_Guide.pdf

Outcomes