AnsweredAssumed Answered

Video encoder Demo code for BF527 showing an exception???

Question asked by sunil@Accord on Apr 18, 2014
Latest reply on Apr 21, 2014 by sunil@Accord

Hi,

    I was running the encoder code on BF527 evaluation kit, The pre-built binary that you have provided is working fine in file I/O mode . But when I run the demo code that you have given, in the Eval-board LED 1 is blinking & showing exception 24 has occurred. The snapshot is attached. Kindly refer to it and help me to overcome this exception ASAP.

 

Its very Urgent.

 

FYI :

1) System is running Windows XP Service pack3 ( 32 bit ).

  2) USB2.0

  3) 3.36GB RAM & Dual core @ 3.3 GHz

4) Eval-board : ADSP-BF527 EZ-KIT LITE 2.2

Regards,

Sunil

Attachments

Outcomes