liangbread

After generating an application LDR with schematic code and parameter,parameter tuning doesn't work

Discussion created by liangbread on Apr 15, 2014
Latest reply on Apr 15, 2014 by JJoseph

Hi everyone,

    I have generated the application LDR with schematic code and parameter,according to "SigmaStudio_No_Download_Mode.pdf" from the FAQ"Is it possible to generate target application LDR file with schematic 'code' and 'parameter' embedded in it?".And it's done with all things going well.But after sharc booted up and music playing,I connect the board to my computer with USBi.Then actions in sigma studio,such as downloading schematic from sigma studio,tuning parameters,just don't work well without any effects.

   For now,I am working on the host controlling to sharc for which downloading from host is no longer needed with the schematic code and parameter embedded in application LDR.So I just question about:

(1)Is it available to send parameters for tuning in this case of parameter and code embedded in application LDR?

(2)Why tuning parameters from sigma studio do not take affect?Any problem with my operation as described above?

Attached is my application project and sigma studio project(sigmastudio version is3.9.2 with SS4S of 2.1.0).

 

Best Regards,

Liang

Attachments

Outcomes