AnsweredAssumed Answered

DTDs for 1920x1080p in Advantive EEdit2.

Question asked by Aphraton on Apr 8, 2014
Latest reply on Jun 4, 2014 by GuenterL

Hello!

In tha Advantive EEdit2 there is a section, that defines EDID DTD, but only a limited number of them.

For example, there is no EDID DTD for 1920x1080x50p and 1920x1080x60p.

What is the solution?

In this post http://ez.analog.com/message/48524#48524 Mattp said, that "I don't think it is necessary to define DTDs."

Do I have to create EDID DTDs for missing 1920x1080x50p and 1920x1080x60p or shall I leave DTD section in Advantive EEdit2 "as is" even if 1920x1080x50p and 1920x1080x60p will be the only allowed modes for the HDMI source?

 

BTW. Even CEA-861-E dosn't have EDID DTD examples for 1920x1080x50p and 1920x1080x60.

If  EDID DTD really doesn't matter, then can I just make EDID DTDs section empty by simply deleting all entries?

Outcomes