AnsweredAssumed Answered

AD9548 vs AD9547

Question asked by Fred1 on Apr 7, 2014
Latest reply on Apr 7, 2014 by neilw

Hi,

 

Is there any difference between the AD9548 and AD9547 apart from the minimum reference frequency and the number of inputs and outputs?

 

The AD9547 is specified with a minimum reference frequency of 1kHz. Would this device be able to lock on a frequency of 1kHz +/-1.5%?

 

If the AD9547 specification has been tested on an AD9548-Eval board, will the same performance be achieved using the actual AD9547 device?

 

Regards,

Fred

Outcomes