AnsweredAssumed Answered

AD9361 IP3

Question asked by james321 on Apr 2, 2014
Latest reply on Apr 10, 2014 by james321

Hi AD9361 expert,

 

AD9361 datasheet gives the overall RX IP3 without external LNA.

I would like to estimate and optimize AD9361 800MHz band IP3 as an external LNA is added.

Could you offer the roughly theoretical input IP3 for ILNA as its gain 21dB and 3dB?

It will be more helpful if you can also offer very rough IP3 for its mixer and LPF at its min gain and max gain?

Your kind help will be greatly appreciated !

Regards,

James

Attachments

Outcomes