AnsweredAssumed Answered

AD9914- Eval board GUI

Question asked by FreddyS on Apr 1, 2014
Latest reply on Apr 2, 2014 by LouijieC

Dear Supporter

Using the AD9914 evalboard with its GUI.

1- Is it possible to jump from profile#1 to profile#8 automatically from the GUI application?

    If not, is there a way to set the PS0-2 pins in the eval board from the GUI?

2- Is there a way to change the phase of the RF signal once it is pulse modulated? (Both phase and amplitude modulations are used at the same time)

Thanks

Outcomes