AnsweredAssumed Answered

UART issue using FMCOMMS2 with KC705 and Microblaze

Question asked by BenG on Mar 31, 2014
Latest reply on Apr 2, 2014 by BenG

After discovering that no project existed for the FMCOMMS2 targeting the KC705 using Microblaze, I decided to build my own. After some time, I finally have the No OS project semi-working. The issue I am seeing is that any command I enter through the UART port results in extra characters being received. For example, if I type "help?", the result is "h0e0l0p0?0" or "hIeIlIpI?I".

 

Has anyone else seen this issue?

Outcomes