AnsweredAssumed Answered

ADL5534 for crystal oscillator?

Question asked by mrln55 on Mar 28, 2014
Latest reply on Mar 31, 2014 by mrln55

In order to develop a series of compact fixed sinewave RF signal sources between 30MHz and 200 MHz, I would like to use the ADL5534 as the basis for a crystal oscillator with a buffer amplifier. Frequency stability and  noise are the primary concerns, absolute frequency accuracy and startup time are not important. The required output level is about 15dBm. Does anybody have any suggestions as to what components would be required to convert Fig. 16 of the ADL5534 datasheet to a crystal oscillator with buffer amplifier, or if there is a better approach? Can this circuit be modeled with the tools available from Analog Devices?

Outcomes