AnsweredAssumed Answered

Regarding In system programming via UART for ADuCM360

Question asked by singhharesh2000@gmail.com on Mar 25, 2014
Latest reply on Mar 25, 2014 by MMA

My data Acquisition system PCB have  one host device communicating with several ADuCM360 ADC devices. All ADuCM360 devices needs to be programmed with different settings. I am planning to use in circuit programming of all  ADuCM360s individually by host device.

 

Now My question is Can i use Digital I/O pins ( 2 pins for each ADuCM360 device) of the host device processor which has enough numbers of digital I/Os, to download the program into ADuCM360s individually.offcourse i will use only two UART pin meant for programming in the ADuCM360 and pull down the boot pin accordingly. Is there any thing i should take care here, because i have yet to get my board. Please correct me if there is better possible way to do it also.

 

I WILL REALLY APPRICIATE YOUR HELP AND SUGGESTION IN THIS REGARD

 

REGARDS,

HARESH

Outcomes