AnsweredAssumed Answered

About AD9361 FDD State configure

Question asked by SPAN on Mar 21, 2014
Latest reply on Mar 25, 2014 by tlili

Dear sir:

 

I want to configure the AD9361 in SPI mode and in FDD state

 

The procedure likes the following:

 

Address      value

0x14            0x65

0x13            0x01

 

I read the 0x17 Reg : it still in the ALERT state ,and setting  0x35: 09  to monitor , Control output [4] ( Tx ON) and [7] ( Rx ON) still stay low.

 

The question is: What is the timing that 0x14 [D5](Force Tx ON) must be set ?  Is 0x65 setting correct?

 

 

Best  Regards,

 

W.T.

Outcomes