AnsweredAssumed Answered

Sigmastudio algorithms

Question asked by gr4eme on Mar 11, 2014
Latest reply on Oct 28, 2014 by dan_xerx

Hi Guys,

 

Im looking to build a couple of features but not sure where to start, There are a lot of blocks to choose from lol

 

Here is what I'm looking to do,

 

First I want to monitor my input signal and if it goes above a set level after say 3 seconds i want it to reduce that level back to a pre determined safe level until the incoming level is reduced.

 

The second thing is monitoring the same input signal and if that signal doubles in level in say .5 second i want to mute the outputs for 5 seconds

 

Looking at the mute block i see it has to be set as either on or off so I'm guessing that i will need to have another block that can be controlled and switch the output from the signal to the mute block

 

Thanks in advance

 

Graeme

Outcomes