AnsweredAssumed Answered

AD8342 question

Question asked by kj.liu on Mar 11, 2014
Latest reply on Mar 21, 2014 by peng.chen

Hi Sir,

 

One of my customer meet an issue in using AD8342 and it needs your help to suggest which direction we could try to solve the problem,

 

Component; ADF4351(central frequency 44MHz, the bandwidth 8MHz and -40dB)  ,AD9857(489MHz and 0dB) ,   AD8342(mix ADF4351 and AD9857)

 

Status: put the ADF4351 output in AD8342 RFIN pin(Pin 15) and AD9857 output in AD8342 LOIN pin(Pin4) and found out that there are no signal in  the AD8342 differential output signal(pin6,pin7) and the T2 RF transformer output. but if they use AD8342 EVB to replace and retest, the signal showed up (differential output is 489MHx , 533MHz and around -40dB) and T2 transformer  (differential output is 489MHx , 533MHz and around -20dB). this picture is shown in Fig.1.

1.jpg

 

Now,the schematic and RC component are all the same as AD8342 EVB setup and the layout looks doesn't have big mistake. If the layout issue , I think the signal would look like the signal is reduced but not all disappear. so I wander to know do you have meet this kind of problem or there is anything we could try. Thank your help!

Outcomes