AnsweredAssumed Answered

Use of AD8307

Question asked by KU3O on Feb 27, 2014
Latest reply on Feb 27, 2014 by jdobler

I've designed and built a scalar network analyzer based on the AD9851 and AD8307.  I intend to submit an article to the QST magazine, but I need to validate some things.  First of all, both components work fabulously.  I implemented the 8307 receivers using the recommendations in the data sheet for a low frequency application (fig. 44), but replaced the shunt capacitor on the input with a 6pf cap that enabled higher frequency cutoff.  But the data sheet says that this configuration (with 5 kohm resistors on the INP and INM leads) should result in an upper limit of an input voltage of 20V.  My unit peaks out at 2.32 v out with a 10V p-p input (50 ohm source). Where am I going wrong?

 

Thanks

Mark

Outcomes