AnsweredAssumed Answered

Sampling Frequency identification

Question asked by gopakumar on Jul 14, 2010
Latest reply on Jul 14, 2010 by Mitesh

Hi,

 

I am using the Ez-Board example SPDIFToAnalogTalkThru(C).

I take in audio through the S/PDIF input for processing and sends the processed audio to the DAC's.

 

The recovered clock from the S/PDIF input is used to drive the Clock and Frame sync's of SPORT's and the DAC's.

 

I would like to know, if it is possible to determine the current sampling frequency of the S/PDIF input in some way so that I can initialize certain coefficients correctly according to the sampling frequency and also configure the DAC correctly.

 

Also, is it possible to detect if there is a change in the sampling frequency of the S/PDIF input so that I can re-configure the DAC's and the re-initialize the coefficients.

 

Can I accomplish the above using the SRC or the PCG or some other modules?

 

Thanks in advance,

 

Gopakumar

Outcomes