AnsweredAssumed Answered

Some questions of ADV7619, again

Question asked by Kaos on Feb 27, 2014
Latest reply on Mar 6, 2014 by Kaos

Dear Sir/Madam, maybe DaveD,

 

I have some questions for your device ADV7619.

 

Please refer to my enclosed file.

 

The chart shows our new design and are going to use ADV7619.

 

Q1.ADV7619 provides two HDMI 1.4 inputs.

We understand that ADV7619 does not support two simultaneous HDMI inputs, correct?

 

Q2.Can the one port of ADV7611 accept an input signal like (1) and (2) on my enclosed?

        (1) and (2) shows half image of 4K2K60p,data rate is 3Gbps.

 

Q3.ADV7619 supports the following format and pixel configuration.( ADV7619_SW_Manual_Rev0.)

     SDR RGB 2 x 24bit interleaved mode

SDR 4:2:2 2 x 16bit interleaved mode

SDR 4:2:2 2 x 20bit interleaved mode

SDR 4:2:2 2 x 24bit  interleaved mode

      We would like to confirm the interleaved output for 3G.

     ex. The chart shows the case of (2 x 24Bit).

interleaved output:

           ->Odd dot out :24Bit

   ->Even dot out :24Bit

->Each interleave output is 960 x 2160.

     Question: Does ADV7619 work like this chart, correct?

 

This question is brought from another sled here due to typo, very sorry.

 

Thanks in advance, Kaos.

Attachments

Outcomes