AnsweredAssumed Answered

No video output from ADV7513

Question asked by Smilence on Feb 26, 2014
Latest reply on Mar 4, 2014 by MikeOC

I met some problems in using ADV7513 in my design.

 

The condition is as following:

Input data: YCbCr 4:2:2 format,

                8bit color depth, embedded Sync,

                and ASP is 16:9, clock 74.25MHz.

                NO Audio data.

And the Data pin connection:

               Y[7:0]-->D[23:16],

               CbCr[7:0]-->D[15:8]

               NO H, V, DE.

According to the PROGRAMMING GUIDE, I think the InputID should be 2, and Style is 3.

 

let's consider a sepcific situation, the input video is 1080_60i

While, I expect the output format is RGB 4:4:4, DVI mode.

 

Now, when powering up the thip, the HPD state(0x42[6]) is HIGH.

Then, I start configure the registers referring to SECTION 3 - QUICK START GUIDE(p14) of the GUIDE.

Here are registers and value that I configured according to my conditon.

Address          Value

0x41[6]          0b0          //Power up circuit.

0x98                             //fixed registers setting.

0x9a

0x9c

0x9d

0xa2

0xa3

0xe0

0xf9          //values as Table 14  Fixed Registers That Must Be Set (Main Map)


//Video input format

0x15[3:0]     0b0010      //Video Format ID = 2

0x16[5:4]     0b11          //Input Color Depth for 4:2:2, 11 = 8 bit

0x16[3:2]     0b11          //Video Input Style, 11 = style 3

0x17[1]        0b1           //Aspect ratio of input video, 16x9 = 0b1


//Video output set

0x16[7]        0b0           //Output Format, 0 for 4:4:4

0x16[0]        0b0           //Output Color Space Selection, 0 = RGB

0x55[6:5]     0b00          //Output format - this should be written when 0x16[7:6], 00 = RGB.

                                   (PS:0x16[6] is reserved 0)

0x17[2]        0b1            //4:2:2 to 4:4:4 Up Conversion Method, 1 = use first order interpolation

0x56[5:0]     0b101010     //Picture Aspect Ratio, 10 = 16:9; Active Format Aspect Ratio, 1010 = 16:9 (center)

                                   (PS: I'm not sure the line above is needed)

0xAF[1]        0b0            //for DVI mode.

 

//HDCP NOT USED.

 

//Color Space Convert

0x18

...

0x2f                         //values referring to Table 32  HDTV YCbCr (Limited Range) to RGB (Limited Range)

 

//DE Generation

0x17[0]      0b1          //Enable DE Generator

0x35

...

0x3a                         //Values referring to Table 26  Register Settings for DE Generation

 

//H, V Sync generation

0x17[6:5]       0b00     //Vsync Polarity, Hsync Polarity

0x30

...

0x34                         //Values referring to Table 28  Register Settings for Embedded Sync Processing

                              (PS: H, V sync. adjustment is not used)

//end

 

I'v tried for several days, but there is no video signal on display(NO SIGNAL, not black green).

FYI.

(1) 0x9e[4] = 0b1, PLL was locked.

     0x3e = 0x14, that means Input VIC Detected was 000101** = VIC#5: 1080i-60, 16:9, which is exactly the input format.

(2) I read out all values of whole register, no error.

(3) I checked the TMDS TCLK+/- signal, and the wave is as the picture shows.

     Its frequency is about 74.25MHz, with an average voltage around 3.0V

OutClock.BMP

(4) And voltage of other Txn+/- pins are around 3.0V. As another 2 picture shows.

TMDS.BMP

TMDS2.BMP

(5) The display only supports up to HDMI 1.3.

(6) The schematic of this part is attached.

 


Attachments

Outcomes