AnsweredAssumed Answered

ADV7393 outputs protection

Question asked by aurelieno on Feb 26, 2014
Latest reply on Feb 27, 2014 by aurelieno

Hi all,

 

I have some questions about the protection we can use on the ADV7393 outputs.

 

I am working on a project which has to convert the video standard STANAG3350. I will use the ADV7393 to do it but I also need to put some "ESD" protection on the outputs to avoid high electrical discharge. The protections need to work from -40°C until 105°C.

 

Do you have any recommendations about these protections I could use?

 

Thanks in advance.

 

Aurélien

Outcomes