AnsweredAssumed Answered

About ADV7341

Question asked by yuji on Feb 23, 2014
Latest reply on Mar 18, 2014 by GuenterL

A value of RSET and RL is prescribed with the data sheet of ADV7341 as follows .

 

For low-drive operation, RSET1 must have a value of 4.12 kΩ, and RL must have a value of 300 Ω.
For full-drive operation, RSET1 must have a value of 510 Ω, and RL must have a value of 37.5 Ω.

 

Can't a setup of those other than this be performed?
When I cannot set it, please tell me the reason.
When you can set it, which value can you use?

 

When I set it in a value of Low-drive mode, it becomes the wave pattern of the blue of the attached file.
Is there the probable cause?

Is it not output like Figure 70-a of data sheet p65?

 

Regards
Yuji

Attachments

Outcomes