AnsweredAssumed Answered

AD-FMCOMMS1-EBZ gets very hot

Question asked by Arne_2 on Feb 20, 2014
Latest reply on Feb 25, 2014 by charlyelkhoury

Hello,

 

I am currently using both, a AD-FMCOMMS1 and an AD-FMCOMMS2 together with my Zedboard.

 

I managed to get Linux bootloaders for both boards and the AD-FMCOMMS2 seems to be working just fine.

 

However, the AD-FMCOMMS1 gets extremely hot (even though it seems to be functioning correctly).

 

I did follow all the startup instructions. In particular, I made sure that the jumper J18 was set to 2.5V as indicated in the Quick Start Guide.

 

I seems that it is not one single component that heats up but rather the entire board (or anything that has silicon in it).

 

Any pointers as to what I should check next?

 

Thanks,

Arne

Outcomes