AnsweredAssumed Answered

ADG1434 Powered Down Properties

Question asked by Wildman on Feb 19, 2014
Latest reply on Feb 20, 2014 by theresaC

Background of Application:


We have 4 independent analog signal lines that range from -12V to 12V coming from an external device.

 

Configuration of ADG1434:


Source Terminals A : Input analog signals from external device

Source Terminals B : Ground

Drain Terminals : Output

 

Questions:


1)  Given the above conditions what natural state would the ADG1434 be in if VDD & VSS are not powered?

 

 

2)  Would applying an input analog signal to Source Terminal A cause damage to an unpowered ADG1434?

Outcomes