AnsweredAssumed Answered

extra data in SigmaStudio

Question asked by genp on Jul 12, 2010
Latest reply on Jul 13, 2010 by BrettG

When I "Link Compile Download" a program to the Sigma DSP,

the capture window shows extra data at the beginning, which are not present

in either darasheet (initialization procedure), or exported files:

 

capture.jpg

Are these data necessary ?

 

Also: I am using ADAU1446.

Since SigmaStudio has only generic ADAU144x device at configuration,

it shows loading data even to the registers not needed for the 1446.

Is it possible to tweak it or do I need to remove unneccessary transfers manually from the microcontroller loading routine ?

 

Thank you,

Gennady

Outcomes