AnsweredAssumed Answered

Analog/Digital(I2S) selectro for ADAU 1702

Question asked by SpeakerDude on Feb 15, 2014
Latest reply on Mar 6, 2014 by Yagami

Hi,

I have a design where I use ADAU1702. I have two audio input sources to my system that I want to be able to select between:

 

Source (1): I2S stereo digital channel from a Bluetooth module

 

Source (2): Analog stereo channel input from a line in jack.

 

I wonder if someone can help me (show a SigmaStudio schematic) how I can implement the following function:

 

Select analog stereo input if I/O#X=high

 

Select I2S digital stereo input if I/O#X=low

 

I will do the same audio processing for the both signals so I just need an I/O-pin-controlled stereo mux.

 

Is pin "2" in the input block the "left channel part" of I2S stereo input (SDATA_IN0) and pin "3" the "right channel part"?

 

Thanks in advance and have a nice weekend!

 

Best regards

Markus

Outcomes