AnsweredAssumed Answered

elfloader stopped working

Question asked by sujan5614 on Feb 15, 2014
Latest reply on Feb 17, 2014 by sujan5614

Hello,

 

I am using CCES v1.0.2 in our project.

 

OS: Windows 7.

 

I am able to successfully build the project and run in debug mode using JTAG. But when I try to create .ldr file it gives the following error:

"elfloader stopped working".

 

The same issue doesn't occur if the host OS is Windows XP, everything works fine. Is there some kind of dependency on Windows 7 for CCES?

 

Our project is in its delivery stage, so please revert back as soon as possible.

 

Regards

Sujan Nag

Outcomes