AnsweredAssumed Answered

ADUM1401 VOD goes momentarily low during power up of VDD2.

Question asked by Jan60 on Feb 14, 2014
Latest reply on Apr 23, 2014 by DaveC

Hello,

 

I'm using the ADUM1401 in an application where VDD1 is up long before VDD2. VID is pulled up to  VDD2 and when I monitor this signal during startup I can see it following VDD2 as expected.

When looking at VOD, this signal is high when VDD2 is unpowered. But during the ramp up of VDD2, a short (5-10 µs) glitch occurs on VOD, which is undesired, because this goes into a falling-edge triggered circuit. What is the cause of this glitch and is there any way to prevent this?

 

Best regards,

 

Jan

Outcomes