AnsweredAssumed Answered

the SPI Communication Problem with ADRF6806

Question asked by yuhd on Feb 11, 2014
Latest reply on Feb 13, 2014 by yuhd

Hi Sir:

I use the adrf6806 for an Energy Metering application.

At first i can lock the 6806,but  after several times i write command, I can not access the spi.

Next is my register set

(

R7=0x000077;
R6=0x1F6106;
R5=0x0000CD;
R4=0x0A17E4;
R3=0x00000B;
R2=0x002162;
R1=0x003001;
R0=0x0002B0;

):

also i can't find the out of REFIN  from MUXOUT when R4=0x8A17E4;

 

I use the FPGA's 3.3V bank access the adrf6806's spi Logic. the rising spur exess 3.6V.

i guess the spur can breakdown the spi logic,how to verify it?

 

Thanks.


Outcomes