AnsweredAssumed Answered

ADV8003, ELPFx, Not using encoder

Question asked by rogerleo on Feb 7, 2014
Latest reply on Feb 11, 2014 by rogerleo

New design.  For the ADV8003 we are not using the Encoder at all.  The Hardware Manual says the ELPFx pins "must be connected" if unused.  I was hoping I would not need to add the RC network shown on the EVAL board.  Can I add a simple PU/PD with just an R or C?  Or do I really need to add the four caps and two resistors?  If so - since we're not using the encoder - are the values critical?  Thank you.

Outcomes